Eaton Logo

If I order a preassembled BladeUPS system with bottom cable entry, then I need to switch it to top cable entry, can I do that?

No, the BladeUPS busbar assembly is specifically designed to handle either top or bottom cable entry points, and can’t be flipped over in the field. However, the 6U wire-way assembly is universal, so it can be relocated in either position. You’d merely need to order the proper busbar assembly for the new configuration.