Eaton Logo

Do communication cards come installed and tested on a preassembled BladeUPS systems?

Yes, allconnectivity cards-- including Web/SNMP, Modbus, Power Xpert UPS, standard relay or industrial relay cards -- will be installed and tested at the factory. The associated external cables for these items are placed, along with the relevant user manual, in an accessory box inside the rear door of the rack during shipment. Additionally, the parallel communications functionality between the individual BladeUPS modules is verified at the factory prior to shipment.