Eaton Logo

What are the extended battery module (EBM) options for the Ferrups FX UPS?

The Ferrups FX comes with several EBM options with varying runtimes in two convenient form factors. Each Ferrups FX features a 20-amp charger standard and can support up to four EBMs to support mission-critical long runtime applications. Click here for more specification information on the Ferrups FX EBMs.