What is the kVA and kW rating of each BladeUPS module?
Each module is rated for 12kVA and/or 12kW. It’s important to note that the kW rating is more important than kVA for this specific product due to the very high power factor (typically .95 - .99) of the computing equipment that BladeUPS is designed to support.