Does the BladeUPS ship with batteries installed?
To ensure the cabinet isn’t damaged by the excess weight of the batteries, BladeUPS modules will ship with the batteries removed. This will also be beneficial for installation since the batteries will not need to be removed from the UPS chassis prior to mounting the system in the IT rack or enclosure. The electronics module and battery packs include a “blind” or self-aligning connector at the rear of each pack, to make them very easy to install or remove.