Can a BladeUPS be paired with a generator?
BladeUPS is a very good option when you need to pair a generator with a UPS. We designed in frequency acceptance windows that help keep the system operating off of the generator, even if the generator isn’t as stable as it should be. This ensures your equipment keeps operating from the generator rather than running the batteries down.