Eaton Logo

Will the BladeUPS system still provide protection if the generator frequency gets erratic?

The BladeUPS system was designed to adapt intelligently to changing conditions such as this. In fact, BladeUPS is smart enough to run unsynchronized with the varying input frequencies, therefore giving the output a stable 60 or 50Hz output frequency. It does this without resorting to battery backup, saving battery capacity for retransfer when utility voltage returns.