If I’m remotely monitoring the BladeUPS system, will the system serial number be visible via my remote connection?
No, your remote connection will pick up the serial number of the individual UPS module you’re talking with, which is the one with the communication card, but not the entire system. It would be best to store the entire system serial number in your asset tracking system, so if service is ever needed, you can reference that number when you call our service hotline.