What mounting options are available for the Eaton High Density rack PDU?
Each high density PDU comes with pre-installed mounting buttons on the back of the PDU, allowing you to simply slide them directly into any industry standard PDU mounting bracket. The PDU also comes with option mounting holes on the side, which allows you to move the buttons for 90 degree side mounting. In this configuration, the outlets face the rear of the enclosure versus the center. This prevents interference in the rail space. If you’re using one of our RS enclosures, the PDU brackets are already installed from the factory. If not no worries, here is the link.