How fast are the alarms coming from the equipment to PredictPulse and the dashboard/mobile app?
One advantage of using email, or SMTP, is its resiliency and speed. In general, all email alarms are real-time and are displayed within seconds of the device transmission, unless unusual Internet or mail server traffic is occurring. PredictPulse dashboards may take as long as 15 minutes to refresh parametric health data based on the system design and device type (or as long as one day for legacy connectivity cards).