Eaton Logo

How can you reduce your cybersecurity risk?

Eaton’s Gigabit Network Card is the first in the industry to receive UL 2900-1 certification, ensuring it has been reviewed and tested, and meets the benchmark of this trusted brand. Encryption and password management are two key enhancements included in the Gigabit Network Card.

Password management:

  • Requires change of password on setup
  • Configurable requirements for password complexity
  • Certificate based authentication in machine to machine connections— no username/password information saved on the client machine, separate certificates for each protocol

Encryption:

  • Uses the most current version of Transport Layer Security protocol (TLS)
  • Only secure protocols enabled by default
  • Firmware is signed and encrypted, and will not boot if tampered with
  • Secure SMTP for email alerts