How can I access the system console in IPM?
- On the IPM 2 OVA, you can access the vCenter remote console or connect via SSH using the OVA’s IP address.
- If you can access the network, you can start an SSH connection. Try to connect on the port 22 (standard SSH port).
- You can log into the system using your credentials.