Eaton Logo

What do I do if my IP address is not set properly IPM?

  • When you configure the network using DHCP, the software may not display the IP address obtained even though it is correctly configured.  If the DNS settings appear correctly, the IP address has also been configured.
  • After the initial wizard network configuration, you need to restart the software in order for the new settings to be applied.
  • When configuring the proxy settings through the initial wizard, please note that it must follow the syntax “http://myProxy@myDomain.com:portNumber”If DHCP is not available, you may configure the network settings from the vCenter console.