Power electronics are the heart of a UPS. They perform the conversion of power from AC to DC and then DC back to AC in a double conversion system. These devices contain the high current, high speed semiconductors that are the hottest, hardest working components of any UPS. Control electronics handle all of the features and functions of the UPS and house the firmware that runs the day to day UPS operation.